Hello,
I use the Sensortag from TI to connect from an IOS Device to the IoT Platform of IBM using the build-in pre-configured Quickstart Connection. The following receipt does not work anymore with the latest TI Apps on IOS. I use the App oftento show clients and students to integrate sensor data into the cloud.
There are 2 versions of the App in the Apple Appstore:
SimpleLink Starter Version 4.92 Build 198
TI SensorTag Version 5 (Build 214)
None of them is able to connect to the IBM IoT Platform Qickstart, only the Android App with Quickstart is working.
The Push to Cloud Slider is working but the Cloud has always the black cross indicating no connections. I tried with IOS 10.2.1 with Ipad and Iphone, no luck. Since it is not possible to install the old App I'm stuck to the Android versions, but a lot of people I will do workshops together with a bunch of sensortags have IPhones.
Thanks for your help in advance,
René Meyer