This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2640: possible bricked CC2640 - best way to recover

Part Number: CC2640


Tool/software: TI-RTOS

Hi,

In trying to get a custom boot loader to work I'vemanaged to make my CC2640 unresponsive to unloading new firmware.

Here's the error I get from within CC studio:

Cortex_M3_0: Error occurred during flash operation: Timed out waiting for target to halt

Cortex_M3_0: Trouble Halting Target CPU: (Error -2062 @ 0x0) Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.407.3)

Another device works fine so I know it not the setup, usb cord, programmer etc etc.

I tried the SmartFR Flash Programmer 2 from inside Parallels on OSX to do a "forced mass erase" but it also errors.

What's the best way to recover from this? I'm using a XDS110 programmer.

Thanks,
Justin