This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564: CC2564b I2S output setup problem

Part Number: CC2564

Hi.

I am trying to set CC2564b to I2S (master).

'HCI_VS_Write_CODEC_Config (0xFD06)' is set as below.
- FSYNC Frequency = 8kHz
- PCM Frequency = 256kHz
- Frame-sync duty cycle = 0
- FSYNC Multiplier = 0X00
- Channel 1 data out size = 16
- Channel 1 data out offset = 1
- Channel 2 data out size = 16
- Channel 2 data out offset = 17

On my board, CC2564b and ATMEL are connected to each other.

When you check with the scope probe, the setting seems to be applied normally.

However, when I hear the HFP voice call, I hear noise.

This noise was the same in the loopback test.

Is there any thing I'm missing?

+) If I set 'FSYNC Frequency = 16kHz', I could hear the sound.

Thank you.