This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2650: Simple_peripheral example doesn't work

Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650

Hi all,

I'm using a CC2650LP and I want to test the device with the simple_peripheral example. I'm using ccs v.7.1. the project is built correctly, no errors occured both in stack and application project but  the device is not found by BLE scanner app. Should I use other App?

I didn't do any change to the CCS options or on the project. Do I have to use OAD System? Why? and how can I do it?

Thanks