We are driving a CC2564MODN (running service pack 1.4) with a TivaC micro. Sometimes we receive a Hardware Error Event from the CC2564B with an error code of 0xB (i.e. UART framing error). We've scoped our transmit signal going to the module and it looks very clean and almost exactly 115.2Kbps (less than 2%, which UARTs typically are fine with). If we receive the Hardware Error Event, we force a complete board reset in 250 ms.
1) Is there any known issue with framing errors on the CC2564B?
2) Does driving the shutdown pin low reset the CC2564B UART? I ask because our board reset drives shutdown low for 10 milliseconds.