This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2650MODA: Application runs fine when FlashROM, But gets Hard Faults when running from OADTarget

Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2640, SYSBIOS, CC2650, CC1350

Tool/software: TI-RTOS

Hi,

I'm having an odd situation where my application runs fine when compiled using 'FlashROM', but gets hard faults at random time, usually between 15 - 30 minutes when is compiled using "OAD target".

Configuration NO_ROM=1,OAD_IMG_E=1 using CCS 7.0. I'm using Bim_extflash as a bootloader. TIRTOS 2.20.1.08 and ble_sdk_2_02_01_18

The application measures the period of a square signal using GPIO interrupts. Strange, but if I increase the frequency signal (500Hz), I usually get the hardfault faster....

I have no hard faults and no issues when running from 'FlashROM'.

Is there something that I'm missing in the cc2640.cfg file? I'm new to TIRTOS, but what I can see from call stack the failures of "knl_Queue" and "knl_Task" would indicate something missing with heap or stack errors? I've tried increasing values (Program.stack and heapMinParams.size) without success. I do not know what else do I need to bring from FlashROM configuration to make it work without hardfaults.

Thanks in advance.

Decoded exception,
Decoded,Hard Fault: FORCED: BUSFAULT: PRECISERR.Data Access Error. Address = 0x41000000
Exception context,
$addr,N/A
$type,ti.sysbios.family.arm.m3.Hwi.ExcContext
threadType,Task
threadHandle,0x20000b64
threadStack,0xb0f9
threadStackSize,45305
r0,0x41000000
r1,0x41000000
r2,0x20001830
r3,0x20001750
r4,0x3
r5,0x20000b64
r6,0x2
r7,0x41000000
r8,0x0
r9,0xc700
r10,0x20001968
r11,0x1
r12,0x2
sp,0x20000c80
lr,0xa20f
pc,0xbc5c
psr,0x21000000
ICSR,0x410803
MMFSR,0x0
BFSR,0x82
UFSR,0x0
HFSR,0x40000000
DFSR,0x0
MMAR,0x41000000
BFAR,0x41000000
AFSR,0x0
Exception call stack,
0    ti_sysbios_knl_Queue_empty__E(struct ti_sysbios_knl_Queue_Object *) at Queue.c:72,PC = 0x0000BC5C FP = 0x20000C80
1    ti_sysbios_knl_Task_blockI__E(struct ti_sysbios_knl_Task_Object *) at Task.c:1213,PC = 0x0000A20E FP = 0x20000C80

this is the CFG file

/******************************************************************************

 @file  cc2640.cfg

 @brief TI RTOS Configuration file for CC26xx

        Imported Symbols
        Note: These symbols are defined following the --cfgArgs option.
        In IAR this is done at the end of the pre-build step.  In CCS, this
        is done in Properties->build->XDCtools-Advanced options->Configuration
        script arguments.  Multiple symbols can be used separating them by a
        comma (",").

        By default, TI RTOS builds with RTOS in ROM, interrupt vectors starting
        at address 0x0 and uses ROM only kernel modules.

        NO_ROM:     When set to a non-zero value, RTOS builds in Flash instead
                    of ROM
        OAD_IMG_A:  When set to a non-zero value, interrupt vectors are set to
                    their expected location for on-chip OAD Image A.
        OAD_IMG_B:  When set to a non-zero value, interrupt vectors are set to
                    their expected location for on-chip OAD Image B.
        OAD_IMG_E:  When set to a non-zero value, interrupt vectors are set to
                    their expected location for external flash OAD.
        USE_EVENTS: Build the RTOS Kernel Event module.

 Group: WCS, BTS
 Target Device: CC2650, CC2640, CC1350

 ******************************************************************************
 
 Copyright (c) 2013-2016, Texas Instruments Incorporated
 All rights reserved.

 Redistribution and use in source and binary forms, with or without
 modification, are permitted provided that the following conditions
 are met:

 *  Redistributions of source code must retain the above copyright
    notice, this list of conditions and the following disclaimer.

 *  Redistributions in binary form must reproduce the above copyright
    notice, this list of conditions and the following disclaimer in the
    documentation and/or other materials provided with the distribution.

 *  Neither the name of Texas Instruments Incorporated nor the names of
    its contributors may be used to endorse or promote products derived
    from this software without specific prior written permission.

 THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
 AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
 THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
 PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
 CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
 EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
 PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
 OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
 WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
 OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
 EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.

 ******************************************************************************
 Release Name: ble_sdk_2_02_01_18
 Release Date: 2016-10-26 15:20:04
 *****************************************************************************/


/* ================ ROM configuration ================ */
/*
 * To use BIOS in flash, comment out the code block below.
 */
if (typeof NO_ROM == 'undefined' || (typeof NO_ROM != 'undefined' && NO_ROM == 0))
{
  var ROM = xdc.useModule('ti.sysbios.rom.ROM');
  if (Program.cpu.deviceName.match(/CC26/)) {
      ROM.romName = ROM.CC2650;
  }
  else if (Program.cpu.deviceName.match(/CC13/)) {
      ROM.romName = ROM.CC1350;
  }
}



/* ================ Boot configuration ================ */
if (typeof NO_ROM == 'undefined' || (typeof NO_ROM != 'undefined' && NO_ROM == 0))
{
  var Boot = xdc.useModule('ti.sysbios.family.arm.cc26xx.Boot');
}
/*
 * This module contains family specific Boot APIs and configuration settings.
 * See the SYS/BIOS API guide for more information.
 */
if (typeof NO_ROM == 'undefined' || (typeof NO_ROM != 'undefined' && NO_ROM == 0))
{
  Boot.driverlibVersion = 2;
  Boot.customerConfig = false;
}


/* ================ Clock configuration ================ */
var Clock = xdc.useModule('ti.sysbios.knl.Clock');
/*
 * When using Power and calibrateRCOSC is set to true, this should be set to 10.
 * The timer used by the Clock module supports TickMode_DYNAMIC. This enables us
 * to set the tick period to 10 us without generating the overhead of additional
 * interrupts.
 *
 * Note: The calibrateRCOSC parameter is set within the Power configuration
 *     structure in the "Board.c" file.
 */
Clock.tickPeriod = 10;
Clock.swiPriority = 5;


/* ================ Types configuration ================ */
var Types = xdc.useModule('xdc.runtime.Types');
/*
 * This module defines basic constants and types used throughout the
 * xdc.runtime package.
 */



/* ================ Defaults (module) configuration ================ */
var Defaults = xdc.useModule('xdc.runtime.Defaults');
/*
 * A flag to allow module names to be loaded on the target. Module name
 * strings are placed in the .const section for debugging purposes.
 *
 * Pick one:
 *  - true (default)
 *      Setting this parameter to true will include name strings in the .const
 *      section so that Errors and Asserts are easier to debug.
 *  - false
 *      Setting this parameter to false will reduce footprint in the .const
 *      section. As a result, Error and Assert messages will contain an
 *      "unknown module" prefix instead of the actual module name.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//Defaults.common$.namedModule = true;
Defaults.common$.namedModule = false;

/* Compile out all Assert's */
//Defaults.common$.diags_ASSERT = Diags.ALWAYS_OFF;

/* Allow Mod_create() and Mod_construct() but not delete() or destruct() */
Defaults.common$.memoryPolicy = Types.CREATE_POLICY;



/* ================ Error configuration ================ */
var Error = xdc.useModule('xdc.runtime.Error');
/*
 * This function is called to handle all raised errors, but unlike
 * Error.raiseHook, this function is responsible for completely handling the
 * error with an appropriately initialized Error_Block.
 *
 * Pick one:
 *  - Error.policyDefault (default)
 *      Calls Error.raiseHook with an initialized Error_Block structure and logs
 *      the error using the module's logger.
 *  - Error.policySpin
 *      Simple alternative that traps on a while(1) loop for minimized target
 *      footprint.
 *      Using Error.policySpin, the Error.raiseHook will NOT called.
 */
//Error.policyFxn = Error.policyDefault;
Error.policyFxn = Error.policySpin;

/*
 * If Error.policyFxn is set to Error.policyDefault, this function is called
 * whenever an error is raised by the Error module.
 *
 * Pick one:
 *  - Error.print (default)
 *      Errors are formatted and output via System_printf() for easier
 *      debugging.
 *  - null
 *      Errors are trapped with a while(1) stub function. This option reduces
 *      code footprint.
 *  - non-null function
 *      Errors invoke custom user function. See the Error module documentation
 *      for more details.
 */
//Error.raiseHook = Error.print;
Error.raiseHook = null;
//Error.raiseHook = "&myErrorFxn";

/*
 * If Error.policyFxn is set to Error.policyDefault, this option applies to the
 * maximum number of times the Error.raiseHook function can be recursively
 * invoked. This option limits the possibility of an infinite recursion that
 * could lead to a stack overflow.
 * The default value is 16.
 */
Error.maxDepth = 2;



/* ================ Hwi configuration ================ */
var halHwi = xdc.useModule('ti.sysbios.hal.Hwi');
var m3Hwi = xdc.useModule('ti.sysbios.family.arm.m3.Hwi');
/*
 * Checks for Hwi (system) stack overruns while in the Idle loop.
 *
 * Pick one:
 *  - true (default)
 *      Checks the top word for system stack overflows during the idle loop and
 *      raises an Error if one is detected.
 *  - false
 *      Disabling the runtime check improves runtime performance and yields a
 *      reduced flash footprint.
 */
//halHwi.checkStackFlag = true;
halHwi.checkStackFlag = false;

/*
 * The following options alter the system's behavior when a hardware exception
 * is detected.
 *
 * Pick one:
 *  - Hwi.enableException = true
 *      This option causes the default m3Hwi.excHandlerFunc function to fully
 *      decode an exception and dump the registers to the system console.
 *      This option raises errors in the Error module and displays the
 *      exception in ROV.
 *  - Hwi.enableException = false
 *      This option reduces code footprint by not decoding or printing the
 *      exception to the system console.
 *      It however still raises errors in the Error module and displays the
 *      exception in ROV.
 *  - Hwi.excHandlerFunc = null
 *      This is the most aggressive option for code footprint savings; but it
 *      can difficult to debug exceptions. It reduces flash footprint by
 *      plugging in a default while(1) trap when exception occur. This option
 *      does not raise an error with the Error module.
 */
//m3Hwi.enableException = true;
//m3Hwi.enableException = false;
m3Hwi.excHandlerFunc = null;

/*
 * Enable hardware exception generation when dividing by zero.
 *
 * Pick one:
 *  - 0 (default)
 *      Disables hardware exceptions when dividing by zero
 *  - 1
 *      Enables hardware exceptions when dividing by zero
 */
m3Hwi.nvicCCR.DIV_0_TRP = 0;
//m3Hwi.nvicCCR.DIV_0_TRP = 1;

/*
 * Enable hardware exception generation for invalid data alignment.
 *
 * Pick one:
 *  - 0 (default)
 *      Disables hardware exceptions for data alignment
 *  - 1
 *      Enables hardware exceptions for data alignment
 */
m3Hwi.nvicCCR.UNALIGN_TRP = 0;
//m3Hwi.nvicCCR.UNALIGN_TRP = 1;

/* Put reset vector at start of Flash */
if (typeof OAD_IMG_A != 'undefined' && OAD_IMG_A == 1)
{
  m3Hwi.resetVectorAddress  = 0x0610;
}
else if (typeof OAD_IMG_B != 'undefined' && OAD_IMG_B == 1)
{
  m3Hwi.resetVectorAddress  = 0x6010;
}
else if (typeof OAD_IMG_E != 'undefined' && OAD_IMG_E == 1)
{
  m3Hwi.resetVectorAddress  = 0x1010;
}
else
{
  m3Hwi.resetVectorAddress  = 0x0;
}

/* Put interrupt vector at start of RAM so interrupts can be configured at runtime */
m3Hwi.vectorTableAddress  = 0x20000000;

/* CC2650 has 50 interrupts */
m3Hwi.NUM_INTERRUPTS = 50;



/* ================ Idle configuration ================ */
var Idle = xdc.useModule('ti.sysbios.knl.Idle');
/*
 * The Idle module is used to specify a list of functions to be called when no
 * other tasks are running in the system.
 *
 * Functions added here will be run continuously within the idle task.
 *
 * Function signature:
 *     Void func(Void);
 */
//Idle.addFunc("&myIdleFunc");



/* ================ Kernel (SYS/BIOS) configuration ================ */
var BIOS = xdc.useModule('ti.sysbios.BIOS');
/*
 * Enable asserts in the BIOS library.
 *
 * Pick one:
 *  - true (default)
 *      Enables asserts for debugging purposes.
 *  - false
 *      Disables asserts for a reduced code footprint and better performance.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//BIOS.assertsEnabled = true;
BIOS.assertsEnabled = false;

/*
 * Specify default heap size for BIOS.
 */
if (typeof NO_ROM == 'undefined' || (typeof NO_ROM != 'undefined' && NO_ROM == 0))
{
  BIOS.heapSize = 1668;
}

/*
 * A flag to determine if xdc.runtime sources are to be included in a custom
 * built BIOS library.
 *
 * Pick one:
 *  - false (default)
 *      The pre-built xdc.runtime library is provided by the respective target
 *      used to build the application.
 *  - true
 *      xdc.runtime library sources are to be included in the custom BIOS
 *      library. This option yields the most efficient library in both code
 *      footprint and runtime performance.
 */
//BIOS.includeXdcRuntime = false;
BIOS.includeXdcRuntime = true;

/*
 * The SYS/BIOS runtime is provided in the form of a library that is linked
 * with the application. Several forms of this library are provided with the
 * SYS/BIOS product.
 *
 * Pick one:
 *   - BIOS.LibType_Custom
 *      Custom built library that is highly optimized for code footprint and
 *      runtime performance.
 *   - BIOS.LibType_Debug
 *      Custom built library that is non-optimized that can be used to
 *      single-step through APIs with a debugger.
 *
 */
BIOS.libType = BIOS.LibType_Custom;
//BIOS.libType = BIOS.LibType_Debug;

/*
 * Runtime instance creation enable flag.
 *
 * Pick one:
 *   - true (default)
 *      Allows Mod_create() and Mod_delete() to be called at runtime which
 *      requires a default heap for dynamic memory allocation.
 *   - false
 *      Reduces code footprint by disallowing Mod_create() and Mod_delete() to
 *      be called at runtime. Object instances are constructed via
 *      Mod_construct() and destructed via Mod_destruct().
 *
 *  When using BIOS in ROM:
 *      This option must be set to true.
 */
BIOS.runtimeCreatesEnabled = true;
//BIOS.runtimeCreatesEnabled = false;

/*
 * Enable logs in the BIOS library.
 *
 * Pick one:
 *  - true (default)
 *      Enables logs for debugging purposes.
 *  - false
 *      Disables logging for reduced code footprint and improved runtime
 *      performance.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//BIOS.logsEnabled = true;
BIOS.logsEnabled = false;

BIOS.swiEnabled = true;



/* ================ Memory configuration ================ */
var Memory = xdc.useModule('xdc.runtime.Memory');
/*
 * The Memory module itself simply provides a common interface for any
 * variety of system and application specific memory management policies
 * implemented by the IHeap modules(Ex. HeapMem, HeapBuf).
 */
/* Create a small "alloc-only" heap */
if (typeof NO_ROM != 'undefined' && NO_ROM != 0)
{
  var HeapMin = xdc.useModule('xdc.runtime.HeapMin');
  var heapMinParams = new HeapMin.Params;
  heapMinParams.size = 1668;
  var myHeapMin = HeapMin.create(heapMinParams);
  Memory.defaultHeapInstance = myHeapMin;
}


/* ================ Program configuration ================ */
/*
 *  Program.stack is ignored with IAR. Use the project options in
 *  IAR Embedded Workbench to alter the system stack size.
 */
if (typeof NO_ROM == 'undefined' || (typeof NO_ROM != 'undefined' && NO_ROM == 0))
{
  Program.stack = 1024;
  Program.argSize = 0;
}
else
{
  Program.stack = 1024; //512; Gaboh: try increasing this
}



/* ================ Semaphore configuration ================ */
var Semaphore = xdc.useModule('ti.sysbios.knl.Semaphore');
/*
 * Enables global support for Task priority pend queuing.
 *
 * Pick one:
 *  - true (default)
 *      This allows pending tasks to be serviced based on their task priority.
 *  - false
 *      Pending tasks are services based on first in, first out basis.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//Semaphore.supportsPriority = true;
Semaphore.supportsPriority = false;

/*
 * Allows for the implicit posting of events through the semaphore,
 * disable for additional code saving.
 *
 * Pick one:
 *  - true
 *      This allows the Semaphore module to post semaphores and events
 *      simultaneously.
 *  - false (default)
 *      Events must be explicitly posted to unblock tasks.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//Semaphore.supportsEvents = true;
Semaphore.supportsEvents = false;




/* ================ Events configuration ================ */
if (typeof USE_EVENTS != 'undefined' && USE_EVENTS != 0)
{
  var Events = xdc.useModule('ti.sysbios.knl.Event');
}



/* ================ Swi configuration ================ */
var Swi = xdc.useModule('ti.sysbios.knl.Swi');
/*
 * A software interrupt is an object that encapsulates a function to be
 * executed and a priority. Software interrupts are prioritized, preempt tasks
 * and are preempted by hardware interrupt service routines.
 *
 * This module is included to allow Swi's in a users' application.
 */
Swi.numPriorities = 6;



/* ================ System configuration ================ */
var System = xdc.useModule('xdc.runtime.System');
/*
 * The Abort handler is called when the system exits abnormally.
 *
 * Pick one:
 *  - System.abortStd (default)
 *      Call the ANSI C Standard 'abort()' to terminate the application.
 *  - System.abortSpin
 *      A lightweight abort function that loops indefinitely in a while(1) trap
 *      function.
 *  - A custom abort handler
 *      A user-defined function. See the System module documentation for
 *      details.
 */
//System.abortFxn = System.abortStd;
System.abortFxn = System.abortSpin;
//System.abortFxn = "&myAbortSystem";

/*
 * The Exit handler is called when the system exits normally.
 *
 * Pick one:
 *  - System.exitStd (default)
 *      Call the ANSI C Standard 'exit()' to terminate the application.
 *  - System.exitSpin
 *      A lightweight exit function that loops indefinitely in a while(1) trap
 *      function.
 *  - A custom exit function
 *      A user-defined function. See the System module documentation for
 *      details.
 */
//System.exitFxn = System.exitStd;
System.exitFxn = System.exitSpin;
//System.exitFxn = "&myExitSystem";

/*
 * Minimize exit handler array in the System module. The System module includes
 * an array of functions that are registered with System_atexit() which is
 * called by System_exit(). The default value is 8.
 */
System.maxAtexitHandlers = 0;

/*
 * The System.SupportProxy defines a low-level implementation of System
 * functions such as System_printf(), System_flush(), etc.
 *
 * Pick one pair:
 *  - SysMin
 *      This module maintains an internal configurable circular buffer that
 *      stores the output until System_flush() is called.
 *      The size of the circular buffer is set via SysMin.bufSize.
 *  - SysCallback
 *      SysCallback allows for user-defined implementations for System APIs.
 *      The SysCallback support proxy has a smaller code footprint and can be
 *      used to supply custom System_printf services.
 *      The default SysCallback functions point to stub functions. See the
 *      SysCallback module's documentation.
 */
//var SysMin = xdc.useModule('xdc.runtime.SysMin');
//SysMin.bufSize = 128;
//System.SupportProxy = SysMin;
var SysCallback = xdc.useModule('xdc.runtime.SysCallback');
System.SupportProxy = SysCallback;
//SysCallback.abortFxn = "&myUserAbort";
//SysCallback.exitFxn  = "&myUserExit";
//SysCallback.flushFxn = "&myUserFlush";
//SysCallback.putchFxn = "&myUserPutch";
//SysCallback.readyFxn = "&myUserReady";



/* ================ Task configuration ================ */
var Task = xdc.useModule('ti.sysbios.knl.Task');
/*
 * Check task stacks for overflow conditions.
 *
 * Pick one:
 *  - true (default)
 *      Enables runtime checks for task stack overflow conditions during
 *      context switching ("from" and "to")
 *  - false
 *      Disables runtime checks for task stack overflow conditions.
 *
 *  When using BIOS in ROM:
 *      This option must be set to false.
 */
//Task.checkStackFlag = true;
Task.checkStackFlag = false;

/*
 * Set the default task stack size when creating tasks.
 *
 * The default is dependent on the device being used. Reducing the default stack
 * size yields greater memory savings.
 */
Task.defaultStackSize = 512;

/*
 * Enables the idle task.
 *
 * Pick one:
 *  - true (default)
 *      Creates a task with priority of 0 which calls idle hook functions. This
 *      option must be set to true to gain power savings provided by the Power
 *      module.
 *  - false
 *      No idle task is created. This option consumes less memory as no
 *      additional default task stack is needed.
 *      To gain power savings by the Power module without having the idle task,
 *      add Idle.run as the Task.allBlockedFunc.
 */
Task.enableIdleTask = true;
//Task.enableIdleTask = false;
//Task.allBlockedFunc = Idle.run;

/*
 * If Task.enableIdleTask is set to true, this option sets the idle task's
 * stack size.
 *
 * Reducing the idle stack size yields greater memory savings.
 */
Task.idleTaskStackSize = 512;

/*
 * Reduce the number of task priorities.
 * The default is 16.
 * Decreasing the number of task priorities yield memory savings.
 */
Task.numPriorities = 6;



/* ================ Text configuration ================ */
var Text = xdc.useModule('xdc.runtime.Text');
/*
 * These strings are placed in the .const section. Setting this parameter to
 * false will save space in the .const section. Error, Assert and Log messages
 * will print raw ids and args instead of a formatted message.
 *
 * Pick one:
 *  - true (default)
 *      This option loads test string into the .const for easier debugging.
 *  - false
 *      This option reduces the .const footprint.
 */
//Text.isLoaded = true;
Text.isLoaded = false;



/* ================ TI-RTOS middleware configuration ================ */
var mwConfig = xdc.useModule('ti.mw.Config');
/*
 * Include TI-RTOS middleware libraries
 */



/* ================ TI-RTOS drivers' configuration ================ */
var driversConfig = xdc.useModule('ti.drivers.Config');
/*
 * Include TI-RTOS drivers
 *
 * Pick one:
 *  - driversConfig.LibType_NonInstrumented (default)
 *      Use TI-RTOS drivers library optimized for footprint and performance
 *      without asserts or logs.
 *  - driversConfig.LibType_Instrumented
 *      Use TI-RTOS drivers library for debugging with asserts and logs enabled.
 */
driversConfig.libType = driversConfig.LibType_NonInstrumented;
//driversConfig.libType = driversConfig.LibType_Instrumented;



// Remaining Modules
var Diags = xdc.useModule('xdc.runtime.Diags');
var Main = xdc.useModule('xdc.runtime.Main');
var Reset = xdc.useModule('xdc.runtime.Reset');





  • Hello Gabohkiin ,

    Can you check your RTOS task stacks for errors in the RTOS Object View (ROV), such as stack overflow?

    Also, one test is to convert your FlashROM build where the RTOS runs in ROM + flash to run with RTOS in flash only. You can define NO_ROM=1 in the .cfg file or project properties, XDCtools, Advanced Options, "Configuration script arguments".

    Best wishes
  • Hi JXS, thanks for replying.

    In regard of RTOS Task Stacks status, I believe it's OK. This is what I have:

    copy and paste from "detailed" tab:

    ,0x200016b8,ti.sysbios.knl.Task.IdleTask,0,Ready,ti_sysbios_knl_Idle_loop__E,0x0,0x0,232,512,0x200020e0,n/a,n/a,
    ,0x20000634,,3,Blocked,gapRole_taskFxn,0x0,0x0,436,896,0x20000688,n/a,n/a,Semaphore: 0x20001eb4
    ,0x20001a60,,5,Blocked,ICall_taskEntry,0xf001,0x20001858,664,952,0x20001ab0,n/a,n/a,Unknown


    copy and paste from "module" tab:

    ,0x20001750,Locked,0x3,false,4,0x20000b64,444,1024,0x20003f48

    Sure, I will try setting NO_ROM=1 in FlashROM build configuration.

    Regards,

    Gaboh

  • Hi JXS,

    I tested the FlashRom build using NO_ROM=1 settings and I didn't see any issues with hard faults. Thank you for that idea, as I went further and continue adding definitions from OADTarget to FlashROM build and found that my project begin to crash when I add FEATURE_OAD in 'predefined symbols' under 'ARM compiler' settings.

    I'll debug code when FEATURE_OAD is defined and search what's really causing these issues.

    Regards,
  • Hi JXS,

    If I comment/suppress all "memcpy" calls or replace them with an alternate method of copying buffers in "oad_target_external_flash.c" file and do not get hardfaults.

    Also, setting oad_target_external_flash.c file with "1 - local optimizations" fixes this, and I do not get hardfaults anymore. The rest of project is set as "4" optimization level.

    I decided to go with latest suggestion.

    Thanks,
    Gaboh