Part Number: CC2640
Hello everyone,
I would like to use BTool as a reference for central role device to analyze maximum throughput data communication for CC2640 chip. I managed to establish the communication link with the BTool and the chip, and made the necessary BLE configurations. I also managed to send the packet with the data, that I wanted to, by pressing "Send" button. However, I could not manage to send the packets one of the other after a short duration repetitively, such as 1 ms or lower. Is there a way to send the packets, such as in a loop (with the expected delay between them if possible)?
Thanks,
Kıvanç Kabasakal