Part Number: CC2650STK
Hi All,
Customers are considering connecting two acceleration sensors to the outside of CC2650STK and evaluating it.
The acceleration sensor is 4-wire SPI I/F.
When CC2650STK + CC-DEVPACK-DEBUG is connected, is it take 2 channels of 4-wire SPI signal from the CC-DEVPACK-DEBUG's test points?
For example, four signals DP0 to DP3 (DIO_23, DIO_24, DIO_25, and DIO_27) and other four signals DP8 to DP11 (DIO_17, DIO_18, DIO_19, DIO_20) are set as the SPI function, Can I communicate with each acceleration sensor?
Is this Correct?
Best Regards,
Takashi