This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2650MODA: The UART's output suddenly becomes weak

Part Number: CC2650MODA


Tool/software: Code Composer Studio

Hi everyone,

I develope the project by using CC2650MODA module. For troubleshootting I try to use the UART output. for this reason I select the two pins for UART RX and TX. According to manual there is no difference in pin selection so I select any empty pins. In this case the pins were DIO_14 for TX and DIO_13 for RX. In the beginning I the UART worked perfectly. The terminal showed everything I needed. but after a period of time the output disapeare. When I tried to connect the scope I saw thet the maximal signal level is  ≈600mV instead of  ≈3V. I tried to configure the other pair of the pins DIO_8 for TX and DIO9 for RX. but it didn't help me at all.

What it maybe the reason? Is it important which pins must be selected for the UART? 

(The project whith which I tested the module is the ZeroProject.)

Thenks for paying attension

Best Regards

Boris Fridman