Part Number: CC2640
Tool/software: TI-RTOS
Hello,
I am running some current consumption tests on a design based on the SimpleBLEPeripheral project and I am experiencing some unexpected behaviour:
Stack: ble_cc26xx_2_01_01_44627
Connection Interval: 162*1.25ms
Timeout: 5000ms
Slave Latency: 0
Link is encrypted.
There is some data generated in a periodic event (1s) that is written in a characteristic via the following line.
Batmon_setParameter((uint8_t) BATMON_VOLTAGE,(uint8_t) BATMON_VOLTAGE_LEN, (void*)voltagedata);
When notifications are enabled for that characteristic the current consumtion stays higher than expected until the next connection event. See attached pictures.
When the caracteristic configuration is set to "00:00" the current consumption stays low between the call of ICall_wait() and the next connection event. Also all the connections have the same distance to each other. When notification is enabled but the line "Batmon_setParameter((uint8_t) BATMON_VOLTAGE,(uint8_t) BATMON_VOLTAGE_LEN, (void*)voltagedata);" is commented out, everything is as expected, too.
The unexpected behaviour can be observed for other characteristics with notifications enabled, too.
I doubt, that this behaviour is intended.
Thanks
Thomas