Part Number: CC2650MODA
Other Parts Discussed in Thread: BOOSTXL-CC2650MA, CC2650
Tool/software: TI-RTOS
Advertising stop randomly
My custom board with CC2650MODA seem to work properly at the begining.
After one hour, its advertising start to stop randomly while other parts of application still working.
I can turn on/off LED or write something via UART, only advertising is not working.
The last state that i got from ***_processStateChangeEvt is GAPROLE_ADVERTISING
My discoverable mode configurations is GAP_ADTYPE_FLAGS_GENERAL
I have tested with CC2650 launchpad and BOOSTXL-CC2650MA, it gives the same result.
I tested SimplePeripheral with my custom board, avertising exist over 12 hours.
I used task profile to see stack usage while running, stack peak is about 600/1024 in my task and 440/440 in GAPRole task.
I tested with GAPRole stack size 768, but i got the same result.
1
Why the advertising can be stopped? because my application is still running and BLE task suppose to run with higher priority.
2
What should i do to toubleshoot the problem?
Best regards,
Sarawin