Part Number: CC2540
Hi,
I'm looking at the feasibility of using the CC2540 in a IoT project where the micro controller will possibly have to be placed in an injection moulded object. The injection moulding will expose the micro controller to temperatures of 185oC and pressure of 15bar for 4 minutes (up to 80 bar pressure during the injection).
Will the micro controller be able to handle these conditions? (I know the max storage temperature is listed as 125oC in the datasheet, but I thought it might be that it can handle higher temperatures for example in a reflow oven.)
Also, where could I get hold of this type of information for other micro controllers if it isn't listed in the datasheet?