This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2640: CCS ERROR

Part Number: CC2640
Other Parts Discussed in Thread: CC2650

Tool/software: Code Composer Studio

Hi All

Device:CC2640F128RHB 5*5(15GPIO) module.

IDE:ccsv7

SDK: ble_sdk_2_02_01_18

Example: Simple_Peripheral_cc2650

i was changed only on macro CC2650DK_7ID to CC2650DK_5XD

// Client Characteristic Configuration UUID
CONST uint8 clientCharCfgUUID[ATT_BT_UUID_SIZE] =
{
LO_UINT16( GATT_CLIENT_CHAR_CFG_UUID ), HI_UINT16( GATT_CLIENT_CHAR_CFG_UUID )
};

When i expand "GATT_CLIENT_CHAR_CFG_UUID " Macro then i got below error

"An internal error occurred during: "Open Declaration".

java.nio.BufferUnderflowException"