Part Number: CC2650
Tool/software: TI-RTOS
Hi,
In sensortag board file I see two I2C ports, 0 and 1.
I was wondering if both of them are real hardware I2C?
I'm just asking because in CC2650 darasheet it doesn't say two I2C ports.
If it has two can I use both of them at the same time in sensor controller? And the performance of both ports are the same?
I have two sensors with same I2C address and instead if changing the address of one of them to use one port I want to have separate ports.
Thanks