This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: Low power setting with UART functions

Part Number: CC2640R2F

Dear all,

customer is doing a uart to ble module with CC2640R2F.

Everytime module is wake up, and  want to use UART and open the uart in code and  get the data, transform the data then close the UART and sleep.

in normal time, the standby power consumption is ok, around 0.1 mA, but sometimes when the UART is closed, but powerconsumption is upto 0.26mA.

then wake the module, open the UART, transform the data and close the UART, the power consumption become 0.1mA again.

Does anyone have comments?

Thanks.