Part Number: CC2640
Hi all,
I need to set a LED inside BIM. For that, added code inside bspSpiOpen(), but LED is not lighting.
External OAD method. is being used
void bspSpiOpen(uint32_t bitRate, uint32_t clkPin)
{
#ifdef BOOT_LOADER
/* GPIO power && SPI power domain */
PRCMPowerDomainOn(PRCM_DOMAIN_PERIPH | PRCM_DOMAIN_SERIAL);
while (PRCMPowerDomainStatus(PRCM_DOMAIN_PERIPH | PRCM_DOMAIN_SERIAL)
!= PRCM_DOMAIN_POWER_ON);
/* GPIO power */
PRCMPeripheralRunEnable(PRCM_PERIPH_GPIO);
PRCMLoadSet();
while (!PRCMLoadGet());
#endif
/* SPI power */
//ROM_PRCMPeripheralRunEnable(PRCM_PERIPH_SSI0);
ROM_PRCMPeripheralRunEnable(PRCM_PERIPH_SSI1);
PRCMLoadSet();
while (!PRCMLoadGet());
IOCPinTypeGpioOutput(IOID_5);
GPIO_setDio(IOID_5);
IOCPinTypeGpioOutput(IOID_27);
GPIO_setDio(IOID_27);
...
...
}
Anything else to be done?
Thanks a lot for help.