Other Parts Discussed in Thread: STRIKE
Hi
SDK2.0.0, CC2640.
It's working well on customer application code which already enable internal watchdog. But It stop working during ESD test.
A reset cycle can recover it, so it don't has hardware damage.
a). Current is continuous ~3mA, VDDR is continuous high level.
b). We are working on follow 9.8 chapter of SWRU393 to check whether CPU jump to exception.
My question is why watchdog don't trigger reset even CPU jump to infinite exception? Watchdog timer is sourcing from 24M to automatic count by hardware timer rather than software and rely on CPU. BTW, it has a 100K frequency drift on 24M cryscal after ESD test.