Other Parts Discussed in Thread: CC2640R2F
Tool/software: Code Composer Studio
Just received a dev kit but can't program it. Wondering if TI didn't program the on-board debugger or if I somehow put it into DFU mode?
Trying to program the LAUNCHXL-CC2640R2 with Code Composer Studio but I can't connect to the on-board XDS110
When I connect the launchxl-cc2640r2 via USB to my computer, it shows up as Tiva Device Firmware Upgrade.
Found this link and was able to program the XDS110 firmware http://processors.wiki.ti.com/index.php/XDS110
cd /Applications/ti/ccsv7/ccs_base/common/uscif/xds110
./xdsdfu -m
./xdsdfu -f firmware.bin -r
After power-cycling the board, it seems to work ok.
Code Composer Studio Version: 7.1.0.00016
MacOS Sierra 10.12.4