Hi,
We have a CC2640R2FRHB based product. I was able to program successfully to our CC2640R2FRHB based product, but the program did not run. I program simple_peripheral and pwm led example program. My steps are below.
- Program simple_peripheral and pwm led example program to CC2640R2F Launchpad and see if it works. (Both program works)
- Program same simple_peripheral and pwm led example program to CC2640R2FRHB based product and see if it works. (Both program did not work)
I tried step 2 several times and it did not work. Our setup is CC-DEVPACK-DEBUG connected to our CC2640R2FRHB based product. Using CCS I have tested JTAG connection to our CC2640R2FRHB based product successfully. The SmartRF Flash Programmer 2 shows successful programming to our CC2640R2FRHB based product, but the program does not run or do not work.
Since, we are using CC2640R2FRHB for our product, are there any changes needed at the program for it to run.
- kel