This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1350: Power consumption

Part Number: CC1350

I'm using the simplePeripheral for the CC1350 Launchpad and changed the intervals below.  We do not attempt any connection.  We are trying to measure the power consumption.

We expect the power to spike a little over 7mA every 10sec for 1 to 2 msec.  It should be in the uA the rest of the time.  However, it is stay at 7mA the whole time.

The build does have POWER_SAVING defined.  We see the advertising every 10sec as expected.  We need to know why the chip isn't going into sleep/power-down.

Any idea?

// Advertising interval when device is discoverable (units of 625us, 160=100ms)
#define DEFAULT_ADVERTISING_INTERVAL 16000

// Limited discoverable mode advertises for 30.72s, and then stops
// General discoverable mode advertises indefinitely
#define DEFAULT_DISCOVERABLE_MODE GAP_ADTYPE_FLAGS_GENERAL

#ifndef FEATURE_OAD
// Minimum connection interval (units of 1.25ms, 80=100ms) if automatic
// parameter update request is enabled
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL 3200

// Maximum connection interval (units of 1.25ms, 800=1000ms) if automatic
// parameter update request is enabled
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL 3200
#else //!FEATURE_OAD
// Minimum connection interval (units of 1.25ms, 8=10ms) if automatic
// parameter update request is enabled
#define DEFAULT_DESIRED_MIN_CONN_INTERVAL 8

// Maximum connection interval (units of 1.25ms, 8=10ms) if automatic
// parameter update request is enabled
#define DEFAULT_DESIRED_MAX_CONN_INTERVAL 8
#endif // FEATURE_OAD

// Slave latency to use if automatic parameter update request is enabled
#define DEFAULT_DESIRED_SLAVE_LATENCY 0

// Supervision timeout value (units of 10ms, 1000=10s) if automatic parameter
// update request is enabled
#define DEFAULT_DESIRED_CONN_TIMEOUT 1000

// Whether to enable automatic parameter update request when a connection is
// formed
#define DEFAULT_ENABLE_UPDATE_REQUEST GAPROLE_LINK_PARAM_UPDATE_INITIATE_BOTH_PARAMS

// Connection Pause Peripheral time value (in seconds)
#define DEFAULT_CONN_PAUSE_PERIPHERAL 6

// How often to perform periodic event (in msec)
#define SBP_PERIODIC_EVT_PERIOD 5000