Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650, CC2650STK, CC2640
Hello, help me to resolve the issue.
We have custom reference board based on CC2650RHB chip with external power supply is 1.8 V. VDDS and VDDR wire have the same voltage is 1.8 V
For debugging we use CC2650 Launch pad with extern power is 1.8V. JTAG lines TMS, TCK, RESET connect to our custom board
But SmartRF flash programmer 2 (ver. 1.7.5) does not see our chip (CC2650RHB) and have state is Unknown
IAR have the same error: Fatal error: Failed to connect to the XDS emulator (connect ICEPick).
If connect CC2650 LaunchPad to CC2650STK board (only TMS, TCK,RESET, GND pins) - all work fine
What is the problem?