Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650
As a starter BLE project I am using the Project Zero for the CC2650 LaunchPad.
I would like to add the Transport Layer to the project <processors.wiki.ti.com/.../Cc2640_Adding_a_UART_or_SPI_driver_to_a_Sample_Project> but there is not enough space. (After following the instructions from the WIKI page, the build fails for lack of space.)
The WIKI actually describes add the TL to the SimpleBLEPeripheral project, which has adequate space.
Why is there so much difference in size between Project Zero and SimpleBLEPeripheral?
Is one of these projects better than the other for a beginning BLE project?
CCS 7.1
BLE 2.2.1.18
TIRTOS 2.20.1.18