This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/CC2541: problem for CC2541 OAD

Part Number: CC2541
Other Parts Discussed in Thread: BLE-STACK

Tool/software: Starterware

dear all:

         I do OAD in the project based on BLE-CC254x-1.4.2.2 protocol stack, with the asymmetric division of IMG_A address and IMG_B, refer to the TI protocol stackBLE-CC254x-1.3.2 HIDAdvRemote_OAD_Large_Img_B, and add predefined files to the XCL project,  

OAD_IMG_A_PAGE=1
OAD_IMG_A_AREA=47
OAD_IMG_B_PAGE=8
OAD_IMG_B_AREA=(124 - OAD_IMG_A_AREA)
FEATURE_OAD_BIM
HAL_IMAGE_B
FEATURE_OAD
OAD_KEEP_NV_PAGES

cc254x_f256_imgB_Large.xcl

the compiler found the following error Error[e16]: Segment ISTACK (size: 0xc0 align: 0) is too long for segment definition. At least 0x6 more bytes needed. The problem occurred while processing the segment placement command "-Z(IDATA)ISTACK+_IDATA_STACK_SIZE#_IDATA_BEG-_IDATA_END", where at the moment of placement the available memory ranges were "IDATA:46-ff"
   Reserved ranges relevant to this placement:
   IDATA:a-1f           VREG
   IDATA:21-38          VREG
   IDATA:39-3a          XSP
   IDATA:3b-3b          DATA_I
   IDATA:3c-43          DATA_Z
   IDATA:44-45          IDATA_Z
   IDATA:46-ff          ISTACK
   BIT:0-7              BREG
   BIT:80-97            SFR_AN
   BIT:a0-af            SFR_AN
   BIT:b8-c7            SFR_AN

How do I solve it?