Fellows,
We have previously successfully applied a CC2650MODA on a very clean design, and following all the guidelines from the datasheet - so there's some experience there already.
On a new project, there are a few space constrains, which made me route the #RST JTAG line going from the pad inwards, and then exiting on the border (image below). Also the TCK and TDO lines run on layer #4, under the pads (ideally I'd run them out of the module limits).
These signals are used only during programming, and should not cause any problems. The antenna region is pristine as per the specs. But better safe than sorry, I'd appreciate to hear confirmation that such won't be an issue (all DRC rules are properly checked and safe clearances are respected).
Regards
Bruno