This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL-CC1350: CC1350 Launchpad Bluetooth won't show up on phone

Part Number: LAUNCHXL-CC1350
Other Parts Discussed in Thread: CC1350

Tool/software: Code Composer Studio

Hi

I'm having some trouble by understanding how to program the CC1350 Launchpad. First of all, i can run and debug the empty_cc1350_LAUNCHXL_tirtos_ccs project on the device and everything seems to work. I can compile and debug the simple_peripheral_cc1350lp_app_FlashROM project, but the device name won't show up on my phone. I have used a Iphone 5 and a Huawei P9 using a BLE-scanner-app on both. Is it possible that i am doing somthing wrong when building the code? when importing the simple_peripheral_cc1350lp_app_FlashROM projec, the simple_peripheral_cc1350lp_stac_FlashROM projec also shows up. I am guessing that it is a split image and i have to gather the two .hex files in to one, but i can't find any documentation on how to do this using the cc1350. In the Project Explorer in CCS there is no documentation about the simple_peripheral_cc1350lp_app_FlashROM projec. 

Second question: has the dual mode RF driver been released? discussed in this thread: https://e2e.ti.com/support/wireless_connectivity/proprietary_sub_1_ghz_simpliciti/f/156/t/525056?tisearch=e2e-sitesearch&keymatch=cc1350 So fare i can see is it not possible to use BLE & Sub-1GHz operation in the same project, which is what I want to do.

Regards

Karsten Schou Nielsen