This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650MODA: CC2650MODA only running in debug mode

Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2650

Hello,

I have ported the multi role project from the Launchpad to the CC2650 Module Bosterpack.
I have done all required steps as recommended in:
http://www.ti.com/lit/an/swra534/swra534.pdf

The application is running in debug mode. But when I stop debug the application is not running. I have tried to power off/on the Launchpad (which supply the boosterpack) after stop debugging. After this the application is also not running.
Have I forgot a signal or anything to start the CC2560MODA?