I have a cc2540 USB dongle and I'm using SmartRF Packet Sniffer 2.18.1.0
I've compiled the project to only advertise on one channel (channel 37) and verified that this is the case.
The packet sniffer can see the advertising packets but no data packets.
I've also tried configuring "connect to initiator address".
(The manual says If this option is not selected, the capture device will start following the first data connection that appears on the current advertising channel - however I've never seen it capture a single packed other than ADV_IND, ADV_NON_CONN_IND and ADV_SCAN_RSP)
I've tried connecting many, many times. The packet sniffer simply isn't seeing anything except advertising packets.
The project doesn't use encryption by the way.
Has anyone managed to make this work?