Part Number: LAUNCHXL-CC2650
Other Parts Discussed in Thread: CC2650
Hi,
A customer ask,
" We are using the CC2650 Launchpad in combination with the Sensor BoosterPack and the Fuel Tank MKII Battery BoosterPack Plug In Module. We encountered the following problem: - We want to read out the sensor values of the Sensor BoosterPack and we tried to use the example codes that are available on the resource explorer. We didn't find the code for the cc2650 LaunchPad but a code example for the MSP-EXP432P401R is available where the pinout should be the same like on the CC2650 Launchpad. We tried to flash this code via the Code Composer Studio (changed the debug target to CC2650) and the flashing procedure was successful. We tried to see the output, so we used the BOOSTXL-SENSORS GUI. At first the gui wasn't able to recognize the board, so we downloaded the latest firmware and we flashed it with the Flash Programmer 2. After the firmware was flashed we started the GUI again and the board was recognized. We chose the right COM-Port but nothing happened. No Sensor values. After this we tried like in the documentation to start the sensor gui and to go to device programming. We got the error message: Error configuring debug server: Error = operation was aborted; the result was that the firmware on the board was destroyed and we needed to flash it again. Do you know what could be the problem?
Can anyone help me with this?
Thank you in advance.