Part Number: CC2640
Other Parts Discussed in Thread: CC2650
I have a question regarding the CC2640 / CC2650 Device Control Panel (SmartRF Studio 7) Features:
We can use the modes "Packet Tx" or "Packet Rx" in SmartRF Studio to send a certain number of packets via fixed channels and collect RSSI samples.
This feature I would like to install in a test firmware on the CC2640.
However, unfortunately, I do not know how SmartRF Studio drives the chip, ie whether it is an embedded function in the "test host" firmware, or an external control via the JTAG port of the XDS110 On-Board Debugger ...
Can you help me with providing some information?
Is there perhaps a kind of short instructions how to get these features implemented quickly and easily in a firmware?
Or is this only possible via the debugger?
In this case, it would be a good to receive a recommendation on how one can collect individual RSSI samples on selectable channels, independent of Advertisement Mode or Connection Mode.