This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650MODA: Module info

Part Number: CC2650MODA
Other Parts Discussed in Thread: CC2640, CC2650

Hi,

I just wanted to get an idea about the differences between the CC2650MODA and CC
2650 itself (such as sensor tag or launchpad.

I see there are just 14 GPIOs on CC2650MODA. Should I use the customized board file for this module? Is there any board file assigned for this module?

For example DIO_5 and 6 are assigned in sensor tag to I2C but is this board to TDI and TDO. 

And I have another question, to program the board just having JATAG_TCK and TMS is enough and I don't need TDI and TDO, am I correct?

Thanks.

  • Hello,

    Please see app note "Running Standalone BLE Applications on CC2650 Module" SWRA534. You can use cJTAG to program the module. See the "CC2640 HW Troubleshooting & Bring Up" article on the TI BLE Wiki - it also applies to the module.

    Best wishes