This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2564MODA: Bluetooth module software support for TMS320F28069M MCU

Part Number: CC2564MODA

Hello,

I am thinking about using TI bluetooth module in my design, but firstly I'd like to clarify a few things.

1) I see there is a Bluetooth Stack available for a few TI MCUs, however I can't find any for Picollo microcontroller that I'm going to use. Is there any kind of API, a ready-to-use libraries that would help me to walk around all the implementation details?

2) Regarding the necessary service pack - is it possible to download it to the Bluetooth device directly from the MCU, without the need of additional configuration through PC?

3) Is there a functional difference between CC2564MODA module and CC2564MODAEM, apart from external COM/EM connectors and integration with evaluation boards? I will be developing an application on DRV8301-69M-KIT platform with Picollo MCU which doesn't seem to be supported, so I'm thinking if there is a sense in buying Bluetooth evaluation board instead of a single module.

Regards

Jakub