This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2541: SimpleBLECentral Multiple Connection.

Part Number: CC2541


HI,

I am using simpleBLECentral code and i want to connect my code with more than one peripheral. So i used below link...

http://processors.wiki.ti.com/index.php/Central_to_MultiPeripherals_V1.4.2 

But i am unable to connect more than one peripheral.

What i did is...First I connect with one and then i am trying to connect with second peripheral but it show connecting only on LCD....it doesn't print connected on LCD and i also put breakpoints but it doesn't hit.  

  • Did you change the value MAX_NUM_BLE_CONNS in the predefined symbols? It seems like it causes the stack to statically allocate more space so you have to be a bit careful about how many connections you want to support.