Part Number: CC2650STK
Other Parts Discussed in Thread: CC2650, , BLE-STACK
Tool/software: Code Composer Studio
Hi everyone. I hope you can clarify me this doubt.
I want to know how fast I can acquire accelerometer data to be sent through BLE (only acelerometer data, not gyroscope or magnetometer).
I have the CC2650 STK, and I have been looking for any information about it but I do not have it clear yet.
I know that the CC2650 is connected with the motion tracking device (MPU-9250) via SPI. According to its datasheet, the MPU-9250 has a maximum output data rate of 4 Khz (so I suppose that it would be possible to acquire data at this frequency), and the accelerometer data size is 16 bits per axis (3 axis) . According to the CC2650 datasheet, the SPI interface supports up to 4 Mhz (so it could be phisically feasible to acquire accelerometer data at 4Khz and have it ready to send in the CC2650)
Another restricting features that we need to take into account is the BLE connection period and the packet size. I have seen in anoher forum thread that the minimum BLE connection period is 7,5 ms, but it would be possible to increase the default MTU size to send more data in a connection event. My doubt about it: is it necessary to stablish a connection every time I send packets over BLE? Is it true that the minimum BLE connection period is 7,5 ms? What is the maximum MTU size?
What I am looking for is the maximum accelerometer data rate that allow us to package this info and send it via BLE using the CC2650STK.
Thank you very much for your support. Any help will be welcome.
Thanks again.