This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F-Q1: GATT request for multiple connections

Part Number: CC2640R2F-Q1
Other Parts Discussed in Thread: CC2640

Dear Experts,

as the TI CC2640 supports multiple connections, is there any limitation regarding the GATT behaviour? For example, while a GATT Write is ongoing on connection #1 is there any blocking point to request another GATT Write or Read on connection #2? Like the Response on one connection must be received until a Write Request can be send on the other connection.

Thanks and best regards,

Gregor