Hi,
I'm currently setting up the SC16IS752 to interface with the CC2541. Instead of Hardware Flow Control (using the RTS and CTS lines), I want to just purely use the TX and RX lines. I also have HostTestRelease flashed onto my CC2541 but I am not sure what I should modify in this project to setup software flow control.
What do I change in the firmware code so that it can send and receive Xon/Xoff bytes so that it knows when it should start listening and interpreting the HCI opcodes that I am sending to the CC2541 Chip?
(I am using the TiWi uB1 chip which has the CC2541. I am not using the EM board either.)
Thanks,
Al