Part Number: CC2564C
Hi
We are working on BLE hub base project where in we are required to connect >8 BLE peripheral devices with the centre BLE hub.
I read CC2564c technical notes wherein it is mentioned that it is supporting 10 simultaneous connections.
But when I am trying to read CC2564c application notes I found description as,
Theoretically, the CC2564C can simultaneously support up to 10 devices (any combination of central and peripherals LE connections). However, when considering real-life scenarios and the Bluetooth specification bandwidth restrictions TI recommends the following conditions for the CC2564C device:
• Acting as a central device for up to three peripherals
• Serving as a peripheral to one central device
Now I am confused if CC2564C will serve my purpose of connecting it to 8 peripheral devices.
Please help.