Other Parts Discussed in Thread: CC2650
Hi, I 've designed my own custom pcb board for CCxx, and I've placed CC2640 IC. I'm providing an input of 3.3 volts as VDD,
and at DC-DC voltage regulator output is around 2.5V. Is it correct? or should it be between 1.7-1.95V?
Should I use cc2650 IC.
When I'm connecting my board with XDS110Jtag debugger to Smart RF flash programmer its shows Unknown. What could be the reason for this.
VDD=3.1V
VDDS = 3V
VDDR=2.48V
Voltage across DCCOUPL cap is 2.9V
I have attatched my design files also.cc2650_design.pdfcc2650 Board design.zip