This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: Bonding information not getting stored in SNV

Part Number: CC2640
Other Parts Discussed in Thread: CC2650

Hi,

my customer is having an issue with getting the bonding information stored in SNV and thus not able to re-use them in the next connection.

He is using the BLE Stack v2 (2.02.01.18) together with the multi_role example.

When using it the multi-role example for the different roles (e.g. peripheral, central, ...) it is not working. If he rebuilds the example for central role only, it works for him. Did You encounter any similar issues or would be able to point into a direction for investigation?

- there is only one connection, so it is not an issue of a full SNV

Many thanks and best regards,

Gregor