This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC2640R2: TX Power Level Software Issue

Part Number: LAUNCHXL-CC2640R2

Hello,

I am currently setting the TX Power Level in Project 0, using the USER_CONFIG.c file. The information needed to set the power level is listed below. However, when setting the power level based on the look up tables, it is very inconsistent with the TI datasheet. At 0dBm ~ 4.8mA, and at 5dBm ~6.2mA.

Defined Component:

Defined Lookup Table:

TX PWR LVL SET:

Any help regarding this issue would be much appreciated.