Part Number: CC2650STK
Other Parts Discussed in Thread: UNIFLASH
Tool/software: Code Composer Studio
I am using CCS (Version: 7.1.0.00016) on MAC. This worked just fine till this week. Now i get the following error during the download process. I download the file using 'debug' icon in CCS. I've validate CCS can recognize the XDS110 debugger and do not see any error.
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: Failed Board Reset: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 6.0.628.1)
Cortex_M3_0: GEL Output: Board Reset Complete.
Error connecting to the target:
(Error -260 @ 0x0)
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the ReadMe.txt file there
for instructions.
(Emulation package 6.0.628.1)
IcePick_C: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 6.0.628.1)
IcePick_C: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 6.0.628.1)
I am still able to download the firmware in FlashROM, just can't debug via FlashOnly_OAD.
Any thoughts on what may be causing the error?
I am using TI XDS110 debug probe. i've read other posts on this error and reviewed http://processors.wiki.ti.com/index.php/Debugging_JTAG_Connectivity_Problems#Lost_control_of_device_execution_state
sincerely appreciate your help