Part Number: CC2640R2F
Hi Team,
I'm trying to integrate the combined stack/app image with our bootloader (BIM.) Things seem to be mostly working -- but after modifying the linker file etc. the system seems to have insufficient memory (this was not the case before modifying the linker file.) Would you be able to take a quick look at our linker file to see what might be going wrong? I also added the following flags to the project (not sure that FEATURE_OAD does anything, since we aren't using the profile, but stuck it in just in case.) I also added HAL_IMAGE_E to the prebuild step.)
Here are the global flags that we've defined:
FEATURE_OAD
HEAPMGR_SIZE=0
HAL_IMAGE_E
BOARD_DISPLAY_USE_LCD=0
BOARD_DISPLAY_USE_UART=1
BOARD_DISPLAY_USE_UART_ANSI=1
CC2640R2_LAUNCHXL
CC26XX
CC26XX_R2
DEVICE_FAMILY=cc26x0r2
xDisplay_DISABLE_ALL
ICALL_EVENTS
ICALL_JT
ICALL_LITE
ICALL_MAX_NUM_ENTITIES=6
ICALL_MAX_NUM_TASKS=3
ICALL_STACK0_ADDR
MAX_NUM_BLE_CONNS=1
STACK_LIBRARY
USE_CORE_SDK
USE_ICALL
xdc_runtime_Assert_DISABLE_ALL
xdc_runtime_Log_DISABLE_ALL