Hi,
I am working on hardware CC2650EM-7ID-RD + SmartRF06 evaluation board. I am using an external analog sensor with the board.I want to implement BLE application to transfer ADC values generated by Tx unit to Rx and using and also interface GUI to display it on Laptop.I have started with simple link Academy tutorial on Task creation and control with the integration of BLE but using different hardware than the one which is given in the tutorial. Can I follow the same tutorial for CC2650EM-7ID-RD + SmartRF06 evaluation board? What are starting steps to develop BLE application?
1)I have started with simple link Academy tutorial on Task creation and control with the integration of BLE but using different hardware than the one which is given in the tutorial. Can I follow the same tutorial for CC2650EM-7ID-RD + SmartRF06 evaluation board?
2)What are starting steps to develop BLE application?
3)Can I use BLE Device manager to monitor the transmission of data?