Hi Sir,
We got a power consumption issue when using CC2541 . Following are the detail description.
(1) Use 2 power supply on the circuit. One is fixed 3.3V that is applied to VCC_3V3. Another one is variable 2.0V~3.0V that is applied to BAT (one end of R2).
(2)When 3.3V power supply is tuned “ON” and BAT is applied to 3.0V as well. CC2541 will do initialization to configure P0.6&P0.7 as input 3-state and going to low power mode.
(3)Tune BAT voltage from 3.0V to 2.0V, and record the VCC_3V3 current consumption as following file.
The result shows the VCC_3V3 current consumption will increase significant when BAT voltage down to 2.0V. Can help to investigate and explain? Thanks.