This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640 Bond count



Hi,

I confuse about the LE bond count, I'm creating a custom pairing procedure between device and APP, I want to use the bond count number to determine the device is already bonded with cell phone at the program started, so my questions..

The bonding list will disappear if I power off the device? If I re-power on the device, then can I just read the bound number while the advertise is not yet broadcasting?

My temp procedure will design like.. Reading the bond number in program start, and if the number more than 0, then don't do the pairing procedure, just directly do the connect action as normal.

And with my pairing procedure, it had some certification, it need to key some combination button on device while doing the pairing, so I need to separate the progress that have / haven't bonded.

Thanks.