This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/CC2640: How to check CPU clock?

Part Number: CC2640

Tool/software: TI-RTOS

Hello everyone,

I'm asking a question that's somehow related to my previous question here,

Our project uses a custom board with a 3.7V lithium battery and the run time performance is critical. The board has a 32 kHz and 24MHz crystals (as the photo below). My question is, how do I check if the main core run off 32 kHz clock most of the time (excluding when it's sleeping)?

Here is a partial of the schematic,

Thanks,

Henry