Part Number: CC2640
Tool/software: TI-RTOS
Hi,
i'm trying to add UART to the Simple Peripheral Projekt out of the SimpleLink 2.01.00 Version.
If i add UART_init(); to main.c it compiles but the device stucks immediately after flashing.
I'm using the correct Board.h for my CC2640F128 5x5.
If i try adding uart to the empty CC2650DK 5XD example, everything works fine.
I'm facing the similar problem which is descripted in this thread:
CC2650 Trying to add Simple to Uart to Simple Peripheral Example
The solution which is provided there, is not enough for my use case.
How can i add UART to my project?
regards Maximilian