I'm trying to figure out why "some" (as in not all of them) Android Devices drop my Bluetooth Low Energy connection after a few seconds.
The behavior within the HCI Snoops reveals the following:
1. LE Create_Connection
2. After 261 ms the Android devices the first time to trigger a LE Connection_Update with values that make sense (Connection Interval min & max 7.5 ms, Latency 0, Supervision Timeout 2000)
3. And recieves success after 560 ms (which seems ok)
4. About 240 ms the Android starts doing a Connection_Update again, but this time it chooses values that do not make sense (Connection Interval Min: 21.25, Connection Interval Max: 45.00, Connection Latency: 0x0000, Supervisor Timeout: 20) which has to result in a disconnect, since the Supervision timeout will trigger a terminate with the Reason "Connection Timeout" (0x08).
5. The terminate happens right after the success message from the slave that the ll connection update request was successful.
Does anyone have an idea how to make android not update the slave latency wrongly (or not do the connection updates at all, which would be fine by me for now).
Does anyone have any idea?
Note: I have seen the noumerous questions regarding these kind of issues, but it seems that noone has provided hard evidence towards the reasons.