This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640: Sensor Controller - Main Cortex M3 not entering low power mode(s)

Part Number: CC2640

TI Friends and Family,

One of our friends is seeing higher current consumption than expected, when running the Sensor Controller on the CC2640.  They believe the main Cortex M3 is not entering a lower power mode when the Sensor Controller is doing its thing.

A huge architectural benefit of the CC2640 is the fact that the Sensor Controller can operate independent of the main M3, for substantial power savings.  We believe there is probably a software setting that is not being enabled that prevents the M3 for entering low power mode when not in use.  Is this something that the user would manually need to configure or could there be something else going on here?

Comments indeed welcomed!  Even if just 2-cent thoughts.  Thank you in advance.

-CY