This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC2650: Sharing Project

Part Number: CC2650


Tool/software: Code Composer Studio

Hi all,

I made some changes to the SimpleBlePeripheral and I am trying to port it to a different PC. The project is working, but when it is imported to a different PC the project stops working when the BLE is active. it does not happen when I build the project on my main PC.

All the files I use are in the project folder and the include-path for the project folder. Any one could have an idea in mind what is causing it works on a PC and not in others.

Changes made:

add two app.c files to the application folder to calculate some equation not a big deal.

the code works only on my PC

Max