This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2650STK: PCA volume purchase and use in end user product

Part Number: CC2650STK
Other Parts Discussed in Thread: CC2650, CC2640R2F

I realize the CC2650STK is only for evaluation and not to be used in an end user product.

Is it possible however to volume purchase the CC2650STK PCA and go through the FCC and bluetooth certification ourselves?

Ideally it would also be nice to not load a few components to help keep costs down.

Doesn't make sense to go through the expense of building a copy of the design when someone else is already setup and sourced the parts to manufacture it.

  • Hello Richard,

    The CC2650STK is a BLE evaluation and prototyping kit and not sold or targeted as an end product. As such, TI does not offer volume purchasing of individual components in the BOM. We do however provide the design files (schematic, layout, BOM and 3D cad files to boot!) which you can use to in the development and certification of your own end product.

    Note that we do recommend you use the CC2640R2F in lieu of the CC2650 if you are targeting a BLE-only design.

    Best wishes
  • Can you provide contact details for the company TI uses to build the CC2650STK development packs?